29 Sept 2023 (Updated at 4:00 pm)
Dear Valued Customer,
Thank you for the long-term support and trust by using Hilti cordless power tools. We always strive to help our customers to maximize the productivity, health and safety and cost efficiency for the work. This is our commitment to our customers.
To further enhance the value that Hilti bring to our customers and the construction industry, we are proud to announce a new cordless tool platform – NURON, with the enormous time and resources investment behind. NURON covers more than 70 tools which can fully replace and outperform our current cordless 22V and 36V platform. This will not only be contributing to the user benefits and experience uplift but also committing to the sustainability development.
The unmatched benefits and feature that NURON cordless tool platform can bring to you:
One platform – From light duty to even floor breaker, it is now all under the same voltage platform and no longer need to keep multiple battery platforms for different applications
Performance – NURON is now bringing impossible to possible that making 15kg weight class floor breaker and gas saw to the platform
Health & Safety – Innovation and advanced technologies in the NURON Cordless Tools further uplift the health and safety standard to next level
Data Driven Services – NURON Tools can now talk and provide data transparency to the user
Meanwhile, Hilti has begun the phase-out of the mentioned current cordless platform with expect completed phase-out date on 31 December 2023. Hilti will provide the assists and alternatives to our customers during the new platform renewal and transition process. In the meantime, warranty and repair services of the current cordless platform will be continued until further notice.
Should you have any questions or need additional information and support, please contact our customer service hotline at 8228-8118 or your Account Manager for details, demonstration, and product trial.
Yours sincerely,
Alison Lee
Head of Marketing
Hilti (Hong Kong) Limited