- Home
- Company
- Company News
- Hilti Blog
Hilti Blog
Discover the latest blog posts on our new product and innovation
Latest Blogs
In Position
In movies, you see protagonists synchronize their watches before operation begins. We do that too, but with a different instrument for a different dimension. If you want every operation to be smooth and done accurately, make sure you align the space first by measuring. PM 30-MG Multi line laser and PM 40-MG Multi line laser are your best partners in doing so.
Read moreCompact 3 lines laser
3 lines laser is not difficult to find in the market, but a 3 lines laser with ±3 mm accuracy within 10m would be harder to find. On top of those, features a compact design, a self-leveling range of ±4.0° at room temperature, maximum 100 m operating distance (diameter) and up to 1.5 days of continuous layout work? You must be looking for PM 30-MG Multi line laser
Read MoreRapid Deployment
Before operation, alignment and leveling has to be done. If you want to finish this step quick, but as accurate, PM 30-MG Multi line laser is your dependable partner. It features fast 360° aligning, levelling and squaring and class 2 laser, which requires no special precautionary measures! Place it, adjust a bit and you are good to go, such rapid deployment will save you much time!
Read MoreScan Before Drill
Why scan before drill?
Because clarity is important. Before you drill, simply scan the wall to reveal all the metal bars behind, avoiding the risks of drill crashing – saves your time, effort and most importantly, enhances safety! Furthermore, after each scan, you can generate a report for the specifiers, making it ever-easy to pass the checks!
Read moreIn the future, time is value
In order to maximize the drilling efficiency, you need to adopt the new technology - PS300 Ferroscan, which can generate structural assessment reports after scanning, not only including statistics but also visual presentation in 2D/3D views of areas! With it, passing QCs are easy and you can bid farewell to those time-consuming paper works before and after operations!
Read moreYour personal radar
Jobsite is a warzone – no matter how many floor plans you have studied, plans always fall behind changes, and you’ll only know that a crash had happened when it happens. Plus, you don’t have that much time to “study”. So, roll your personal radar out and scan every inch, and be omniscient about the wall. Work accurate and fast with perfect information!
Read more300mm scan depth
Between the 300mm PS1000 X-SCAN scanning depth, there will be no secret. It locates multi-layers of rebar, tendon, metal and plastic conduit, glass-fiber cable, void and wood in dry concrete structure, giving you the most accurate information of the walls on-site!
Read moreVisualize the dimensions with just one scan
Reduce time for quality checks and composition of assessment reports with PS1000 X-SCAN plus PROFIS Detection Office! Simply scan once and import the data into the software to visualize in 2D and 3D plan views or cross-sectional images, and automatically generate various calculation and visualization parameters!
Read moreSponsor to be evolve
The business field is as cruel as the battlefield, but luckily, we are sponsor to be evolve – introducing Construction Innovation and Technology Fund (CITF). PS1000 X-SCAN is listed on the Construction Innovation and Technology Fund’s pre-approved list.
Read more