- 主頁
- 行業解決方案
- 設計中心
- 防火解決方案 (英文版本)
- Customer Project Aalborg
University Hospital in Aalborg, Denmark
Workable firestop solutions for a major modern hospital
![Customer Project Aalborg Denmark](/content/hilti/A1/HK/zh/business/design-center/fire-protection/customer-project-aalborg/_jcr_content/pagestageimage.img.1920.medium.jpg/1565860680503.jpg)
University Hospital is the centerpiece of ambitious plans to centralize all existing regional healthcare facilities under one roof. The complex encompasses 581 beds, 32 operating rooms, 117 outpatient facilities, 27 daycare facilities and 29 imaging rooms spread across 150,000 m2.
The challenge
![Cast-in device and speed sleeve for hospital firestop solution](/content/hilti/A1/HK/zh/business/design-center/fire-protection/customer-project-aalborg/_jcr_content/mainSection/mainColumn/image_text/image.img.1920.medium.png/1565860679647.png)
Future-proofing firestop despite routine cable retrofitting
When it comes to fire safety, hospitals are uniquely challenging projects. On the one hand, variations in the mobility of occupants means that evacuation times must be maximized. On the other, modern hospitals contain complex and ever-changing building services installations. This demands passive fire safety and compartmentation measures which can meet the strictest regulations, but also allow downtime-free maintenance of pipes/cables. The new University Hospital in Aalborg has been designed for these uncompromising safety and flexibility specifications.
The Building Owner’s main concern was to make sure that all firestop is installed correctly and easy to maintain. Future-proofing was also a key goal – the integrity of all firestop must be preserved despite routine cable retrofitting. On top of that, ongoing value engineering and schedule optimization demanded a user-friendly, high-productivity firestop proposal.
Kim Enevold, Design Engineer
Oluf Jørgensen, Consulting Engineers
Our solution
![CFS-SL GA Firestop Speed Sleeve](/content/hilti/A1/HK/zh/business/design-center/fire-protection/customer-project-aalborg/_jcr_content/mainSection/mainColumn/image_text_copy/image.img.1920.medium.jpg/1565860679858.jpg)
Start planning firestop early
It is never too early to start planning firestop, and this project is case-in-point. From the design phase, Hilti Project Engineers worked directly with Specifiers to develop a firestop solution tailored to not only the budget and schedule, but also the practicalities of the hospital once it is operational. The Building Owner’s safety requirements could be met without compromising the project delivery time, cable management, airflow control and product approvals.
During the construction phase, a dedicated Hilti Project Team routinely visited the jobsite to provide installation guidance and support to the Contractor’s team. Any challenges could be tackled on-site, helping to avoid causing delays or overruns.
5,000 CFS-CID cast-in devices and 10,000 CFS-SL speed sleeves make up the finished hospital’s fire compartmentation plan. For pipe penetrations, the CFS-CID cast-in device was selected as it reduces construction time and cost overall, and virtually guarantees fully approved firestopping when installed correctly. For firestopping cables, speed sleeves were specified thanks to their airflow control and because they make replacing cables a quick and cost-effective task for Facility Managers.